Part Number: AM6548
Hi TI
we are using icssg driver for the am6548. and currently we are facing some ethernet issues.
currently, we use icssg0. icssg driver and prufw are from sdk8.0.
we use icssg0 and there are two ethernet ports.
Below picture shows our reproduce setup.

Port1 configure dhcp and port2 configure as static ip.
After several times reboot, static ip port can not ping each other, but dhcp port works normally.
after debug, found the rx packet of static port is zero. as blow picture.



Could you pls help to debug and solve this issue?
thanks a lot