This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA4VM: How can I reduce the time spent on the Display nodes

Part Number: TDA4VM

Hi TI,

We are working on the TDA4 , SDK 0703.

We use the display node to display 1920*720*2 image.(Image size is 1920 * 720 * 2)

The performance is as below:

About 45 fps.


NODE: CAPTURE1: capture_node: avg = 1484 usecs, min/max = 98 / 3381862 usecs, #executions = 21501
NODE: DISPLAY2: display_node: avg = 20929 usecs, min/max = 14836 / 45226 usecs, #executions = 21501
NODE: DISPLAY1: display_node: avg = 20906 usecs, min/max = 74 / 27336 usecs, #executions = 21501

So , is there any solution to reduce the display node time?

Thanks a lot !