Part Number: TDA4VM
I'm running PSDK 8.02 with a 10-bit raw (RGB), 2560x1984 resolution camera.
I have set up the camera such that it is streaming - and I can save a capture and see the raw image - but the display shows nothing but a fixed pattern of noise: white screen - black speckles - does not respond to changes in the camera input, and does not change. Sometimes, a singular grey-scale image will pop up on the monitor, then it will promptly go back to that previously mentioned static screen. I'm assuming this is an issue with the DCC files? or have I missed something?
I have tried various different DCC configuration setups, as well as lowering the ROI so that the output image is smaller, but nothing changes the symptoms I see. Before tampering with it I expected to at least see a darker-than-usual image because of it's bit-depth, but I did not expect to see an unresponsive display.