This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

error: can't open engine XXXXX

Hi,

when i test my codec, I got a segmentation failed error, then the program exited.

If I try to run this program again, I will get a error 

-----------------------------------------------------------------------------------------------------------

Assertion at Line no: 384 in /Arago/netra/arago-tmp/work/c6a816x-evm-none-linux-

gnueabi/ti-syslink-02_00_00_56-r1i/syslink_02_00_00_56_alpha2/ti/syslink/utils/h

los/knl/Linux/../../../../../../ti/syslink/ipc/hlos/knl/Linux/HeapBufMPDrv.c: (c

args.args.create.handle != NULL) : failed

./app_remote.xv5T: error: can't open engine XXXXX

-----------------------------------------------------------------------------------------------------------

I think this because the program quit, but the engine is still opening.

I can just restart the board to debug it again.

Is there any method to force-close the opening engine or any other method to make the debug easier?

 

yours,

wang