Hi Team,
Development board: TDA4VM
Expansion board: Fusion1 Board
Sensor: IMX623-UB953_SONY
Situation: The same software detected 'J7X-BASE-CPB rev E2', 'J7X-INFOTAN-EXP rev E3', and 'J7X-VSC8514-ETH rev E2' in U-Boot SPL 2019.01-g350f3927b8 (Feb 17 2020 - 09:48:06 +0000). It was trying to boot from MMC2.
SoC: J721E PG 1.0
Model: Texas Instruments' K3 J721E SoC
Board: It could run smoothly on the hardware of the J721EX-PM1-SOM rev E2 version
On U-Boot SPL 2019.01-g350f3927b8 (Feb 17 2020 - 09:48:06 +0000), it detected 'J7X-BASE-CPB rev A' and 'J7X-VSC8514-ETH rev E2'. It was trying to boot from MMC2.
SoC: J721E PG 2.0
Model: Texas Instruments' K3 J721E SoC
Board: It did not run smoothly on the hardware of the J721EX-PM2-SOM rev A version.
The whole log is in the attached document.
Question: What are the specific differences between the hardware of the two versions, and do I need to make any modifications in the configurations of the software?
The software we used for testing is the single camera demo provided by TI vision app, and modifications have been made on this basis.