Part Number: AM3352
Hello,
I tried to install "usermod" command, but got fail. (I'm using SDK8.2.)
I added "shadow-sysroot" to IMAGE_INSTALL_append in local.conf, and executed build command of bitbake like "bitbake tisdk-base-image".
Then, I got an error as following. ( The attached file are the complete log file and the local.conf which I'm using. )
ERROR: Task do_populate_sdk in /home/rmu/tisdk2/sources/meta-arago/meta-arago-distro/recipes-core/images/tisdk-base-image.bb rdepends upon non-existent task do_package_write_ipk in /home/rmu/tisdk2/sources/oe-core/meta/recipes-extended/shadow/shadow-sysroot_4.6.bb ERROR: Command execution failed: 1
Could you teach me how to install "usermod" command ?
NOTE: Started PRServer with DBfile: /home/rmu/tisdk2/build/cache/prserv.sqlite3, IP: 127.0.0.1, PORT: 34967, PID: 21045 NOTE: Resolving any missing task queue dependencies WARNING: preferred version 2.32% of nativesdk-glibc-locale not available (for item nativesdk-glibc-locale) WARNING: versions of nativesdk-glibc-locale available: 2.35 WARNING: preferred version 2.32% of nativesdk-glibc-locale not available (for item nativesdk-glibc-localedatas) WARNING: versions of nativesdk-glibc-locale available: 2.35 WARNING: preferred version 2.32% of nativesdk-glibc-locale not available (for item nativesdk-glibc-charmaps) WARNING: versions of nativesdk-glibc-locale available: 2.35 WARNING: preferred version 9.2% of gdb not available (for item gdbserver) WARNING: versions of gdb available: 9.1 WARNING: preferred version 2.32% of nativesdk-glibc-locale not available (for item nativesdk-glibc-gconvs) WARNING: versions of nativesdk-glibc-locale available: 2.35 WARNING: preferred version 2.32% of nativesdk-glibc not available (for item virtual/nativesdk-libiconv) WARNING: versions of nativesdk-glibc available: 2.35 WARNING: preferred version 2.32% of nativesdk-glibc not available (for item virtual/nativesdk-libc) WARNING: versions of nativesdk-glibc available: 2.35 WARNING: preferred version arm-9.2% of gcc-crosssdk-x86_64-arago-linux not available (for item virtual/x86_64-arago-linux-gcc-crosssdk) WARNING: versions of gcc-crosssdk-x86_64-arago-linux available: 12.1.0 arm-11.2 WARNING: preferred version 2.35% of binutils-crosssdk-x86_64-arago-linux not available (for item virtual/x86_64-arago-linux-binutils-crosssdk) WARNING: versions of binutils-crosssdk-x86_64-arago-linux available: 2.34 WARNING: preferred version 2.32% of nativesdk-glibc not available (for item virtual/nativesdk-libintl) WARNING: versions of nativesdk-glibc available: 2.35 WARNING: preferred version arm-9.2% of nativesdk-gcc-runtime not available (for item virtual/nativesdk-x86_64-arago-linux-compilerlibs) WARNING: versions of nativesdk-gcc-runtime available: 12.1.0 arm-11.2 WARNING: preferred version 2.32% of nativesdk-glibc not available (for item nativesdk-glibc-utils) WARNING: versions of nativesdk-glibc available: 2.35 WARNING: preferred version 2.32% of nativesdk-glibc-locale not available (for item nativesdk-glibc-gconv-ibm851) WARNING: versions of nativesdk-glibc-locale available: 2.35 WARNING: preferred version 2.32% of nativesdk-glibc-locale not available (for item nativesdk-glibc-gconv-ibm865) WARNING: versions of nativesdk-glibc-locale available: 2.35 WARNING: preferred version arm-9.2% of nativesdk-libgcc not available (for item nativesdk-libgcc) WARNING: versions of nativesdk-libgcc available: 12.1.0 arm-11.2 WARNING: preferred version 2.32% of nativesdk-glibc-locale not available (for item nativesdk-glibc-gconv-ibm737) WARNING: versions of nativesdk-glibc-locale available: 2.35 WARNING: preferred version 2.32% of nativesdk-glibc-locale not available (for item nativesdk-glibc-gconv-ibm869) WARNING: versions of nativesdk-glibc-locale available: 2.35 WARNING: preferred version 2.32% of nativesdk-glibc-locale not available (for item nativesdk-glibc-gconv-ibm850) WARNING: versions of nativesdk-glibc-locale available: 2.35 WARNING: preferred version 2.32% of nativesdk-glibc-locale not available (for item nativesdk-glibc-gconv-ibm862) WARNING: versions of nativesdk-glibc-locale available: 2.35 WARNING: preferred version 2.32% of nativesdk-glibc-locale not available (for item nativesdk-glibc-gconv-ibm857) WARNING: versions of nativesdk-glibc-locale available: 2.35 WARNING: preferred version 2.32% of nativesdk-glibc not available (for item nativesdk-ldconfig) WARNING: versions of nativesdk-glibc available: 2.35 WARNING: preferred version 2.32% of nativesdk-glibc-locale not available (for item nativesdk-glibc-gconv-ibm866) WARNING: versions of nativesdk-glibc-locale available: 2.35 WARNING: preferred version 2.32% of nativesdk-glibc-locale not available (for item nativesdk-glibc-gconv-ibm437) WARNING: versions of nativesdk-glibc-locale available: 2.35 WARNING: preferred version 9.2% of gdb not available (for item gdb-dev) WARNING: versions of gdb available: 9.1 WARNING: preferred version 2.32% of nativesdk-glibc not available (for item nativesdk-glibc-dev) WARNING: versions of nativesdk-glibc available: 2.35 WARNING: preferred version 9.2% of gdb not available (for item gdb) WARNING: versions of gdb available: 9.1 WARNING: preferred version 2.32% of nativesdk-glibc-locale not available (for item nativesdk-glibc-gconv-ibm852) WARNING: versions of nativesdk-glibc-locale available: 2.35 WARNING: preferred version 2.32% of nativesdk-glibc-locale not available (for item nativesdk-glibc-gconv-ibm863) WARNING: versions of nativesdk-glibc-locale available: 2.35 WARNING: preferred version 2.32% of nativesdk-glibc-locale not available (for item nativesdk-glibc-gconv-ibm855) WARNING: versions of nativesdk-glibc-locale available: 2.35 WARNING: preferred version 2.32% of nativesdk-glibc-locale not available (for item nativesdk-glibc-gconv-ibm861) WARNING: versions of nativesdk-glibc-locale available: 2.35 WARNING: preferred version 2.32% of nativesdk-glibc-locale not available (for item nativesdk-glibc-gconv-ibm860) WARNING: versions of nativesdk-glibc-locale available: 2.35 WARNING: preferred version 2.32% of nativesdk-glibc-locale not available (for item nativesdk-glibc-gconv-ibm775) WARNING: versions of nativesdk-glibc-locale available: 2.35 WARNING: preferred version arm-9.2% of nativesdk-libgcc not available (for item nativesdk-libgcc) WARNING: versions of nativesdk-libgcc available: 12.1.0 arm-11.2 WARNING: preferred version arm-9.2% of gcc-crosssdk-x86_64-arago-linux not available (for item virtual/x86_64-arago-linux-g++-crosssdk) WARNING: versions of gcc-crosssdk-x86_64-arago-linux available: 12.1.0 arm-11.2 WARNING: preferred version arm-9.2% of nativesdk-libgcc-initial not available (for item nativesdk-libgcc-initial) WARNING: versions of nativesdk-libgcc-initial available: 12.1.0 arm-11.2 Build Configuration: BB_VERSION = "1.46.0" BUILD_SYS = "x86_64-linux" NATIVELSBSTRING = "ubuntu-16.04" TARGET_SYS = "arm-linux-gnueabi" MACHINE = "am335x-evm" DISTRO = "arago" DISTRO_VERSION = "2021.09" TUNE_FEATURES = "arm armv7a vfp thumb neon callconvention-hard" TARGET_FPU = "hard" meta-processor-sdk = "rmu:30695ba2c22b83c1d442b09955dfe865767db646" meta-arago-distro meta-arago-extras = "rmu:bc567268b90f7c9b62c8d603c97df669f8ee59ca" meta-qt5 = "rmu:d5083424cae7bfb6cabff4bc285dd5c33cc464c1" meta-virtualization = "rmu:080cae941a8d85495ebeeee548be17cf423cb9c8" meta-networking meta-python meta-oe meta-gnome meta-filesystems meta-webserver = "rmu:780cd4eb9e146dabf5873b027018a509c53994d9" meta-ti = "rmu:190993365e27ed69f15b24373ecdf41e11ad46a2" meta-arm meta-arm-toolchain = "rmu:b2f964b379c8c24ac962db42a08ec58634dd20cb" meta = "rmu:01895493297f7cab01d0a2fabb9336d3dcbd579b" ERROR: Task do_populate_sdk in /home/rmu/tisdk2/sources/meta-arago/meta-arago-distro/recipes-core/images/tisdk-base-image.bb rdepends upon non-existent task do_package_write_ipk in /home/rmu/tisdk2/sources/oe-core/meta/recipes-extended/shadow/shadow-sysroot_4.6.bb ERROR: Command execution failed: 1
# CONF_VERSION is increased each time build/conf/ changes incompatibly
CONF_VERSION = "1"
#
# Where to place downloads
#
# During a first build the system will download many different source code
# tarballs from various upstream projects. This can take a while, particularly
# if your network connection is slow. These are all stored in DL_DIR. When
# wiping and rebuilding you can preserve this directory to speed up this part
# of subsequent builds. This directory is safe to share between multiple builds
# on the same machine too.
DL_DIR = "/home/rmu/tisdk2/downloads"
#
# Where to place shared-state files
#
# BitBake has the capability to accelerate builds based on previously built
# output. This is done using "shared state" files which can be thought of as
# cache objects and this option determines where those files are placed.
#
# You can wipe out TMPDIR leaving this directory intact and the build would
# regenerate from these files if no changes were made to the configuration.
# If changes were made to the configuration, only shared state files where the
# state was still valid would be used (done using checksums).
SSTATE_DIR = "${OEBASE}/build/sstate-cache"
#
# Shared-state files from other locations
#
# As mentioned above, shared state files are prebuilt cache data objects which
# can be used to accelerate build time. This variable can be used to configure
# the system to search other mirror locations for these objects before it
# builds the data itself.
#
# This can be a filesystem directory, or a remote url such as http or ftp.
# These would contain the sstate-cache results from previous builds (possibly
# from other machines). This variable works like fetcher MIRRORS/PREMIRRORS
# and points to the cache locations to check for the shared objects.
#SSTATE_MIRRORS ?= "\
#file://.* http://someserver.tld/share/sstate/ \n \
#file://.* file:///some/local/dir/sstate/"
#
# Where to place the build output
#
# This option specifies where the bulk of the building work should be done and
# where BitBake should place its temporary files and output. Keep in mind that
# this includes the extraction and compilation of many applications and the toolchain
# which can use Gigabytes of hard disk space.
TMPDIR = "${TOPDIR}/arago-tmp"
# By default, DEPLOY_DIR is inside TMPDIR, but can be changed here to be outside
#DEPLOY_DIR = "${TOPDIR}/deploy"
#
# Machine Selection
#
# You need to select a specific machine to target the build with. There are a selection
# of emulated machines available which can boot and run in the QEMU emulator:
#
MACHINE ?= "am335x-evm"
#
# Package Management configuration
#
# This variable lists which packaging formats to enable. Multiple package backends
# can be enabled at once and the first item listed in the variable will be used
# to generate the root filesystems.
# Options are:
# - 'package_deb' for debian style deb files
# - 'package_ipk' for ipk files are used by opkg (a debian style embedded package manager)
# - 'package_rpm' for rpm style packages
# E.g.: PACKAGE_CLASSES ?= "package_rpm package_deb package_ipk"
# We default to ipk:
PACKAGE_CLASSES ?= "package_ipk"
#
# SDK/ADT target architecture
#
# This variable specified the architecture to build SDK/ADT items for and means
# you can build the SDK packages for architectures other than the machine you are
# running the build on (i.e. building i686 packages on an x86_64 host._
# Supported values are i686 and x86_64
SDKMACHINE ?= "x86_64"
#
# Extra image configuration defaults
#
# The EXTRA_IMAGE_FEATURES variable allows extra packages to be added to the generated
# images. Some of these options are added to certain image types automatically. The
# variable can contain the following options:
# "dbg-pkgs" - add -dbg packages for all installed packages
# (adds symbol information for debugging/profiling)
# "dev-pkgs" - add -dev packages for all installed packages
# (useful if you want to develop against libs in the image)
# "tools-sdk" - add development tools (gcc, make, pkgconfig etc.)
# "tools-debug" - add debugging tools (gdb, strace)
# "tools-profile" - add profiling tools (oprofile, exmap, lttng valgrind (x86 only))
# "tools-testapps" - add useful testing tools (ts_print, aplay, arecord etc.)
# "debug-tweaks" - make an image suitable for development
# e.g. ssh root access has a blank password
# There are other application targets that can be used here too, see
# meta/classes/image.bbclass and meta/classes/core-image.bbclass for more details.
# We default to enabling the debugging tweaks.
EXTRA_IMAGE_FEATURES = "debug-tweaks tools-debug read-only-rootfs ssh-server-openssh"
IMAGE_INSTALL_append = " gdbserver openssh-sftp-server net-snmp net-snmp-server net-snmp-dev nodejs mmc-utils rsyslog sqlite3 ntp ntpdate tree python3-flask python3-django python3-djangorestframework tzdata procps python3-pytest python3-pip python3-gunicorn nginx zip unzip rsync perl-module-io-file perl-module-data-dumper perl-module-file-copy perl-module-net-smtp perl-module-posix perl-module-file-temp perl-module-filehandle shadow-sysroot"
VOLATILE_LOG_DIR = "no"
TARGET_CPPFLAGS += "-D_TIME_BITS=64 -D_FILE_OFFSET_BITS=64"
#
# Additional image features
#
# The following is a list of additional classes to use when building images which
# enable extra features. Some available options which can be included in this variable
# are:
# - 'buildstats' collect build statistics
# - 'image-mklibs' to reduce shared library files size for an image
# - 'image-prelink' in order to prelink the filesystem image
# - 'image-swab' to perform host system intrusion detection
# NOTE: if listing mklibs & prelink both, then make sure mklibs is before prelink
# NOTE: mklibs also needs to be explicitly enabled for a given image, see local.conf.extended
USER_CLASSES ?= "buildstats image-mklibs image-prelink"
# By default disable interactive patch resolution (tasks will just fail instead):
PATCHRESOLVE = "noop"
# Qemu 0.12.x is giving too much problems recently (2010.05), so disable it for users
ENABLE_BINARY_LOCALE_GENERATION = "0"
# By default the machine configuration file sets the IMAGE_FSTYPES. But if you
# would like to add additional file system types you can uncomment the
# following line and add the additional IMAGE_FSTYPES you want created
# as part of the build flow. Some common types are listed below and you
# can remove the ones you do not want.
# IMAGE_FSTYPES += "jffs2 cramfs ext2.gz ext3.gz squashfs ubi tar.gz tar.bz2 cpio"
#
# Parallelism Options
#
# These two options control how much parallelism BitBake should use. The first
# option determines how many tasks bitbake should run in parallel:
#
BB_NUMBER_THREADS ?= "3"
#
# The second option controls how many processes make should run in parallel when
# running compile tasks:
#
PARALLEL_MAKE ?= "-j 3"
#
# For a quad-core machine, BB_NUMBER_THREADS = "4", PARALLEL_MAKE = "-j 4" would
# be appropriate for example
DISTRO = "arago"
# Set terminal types by default it expects gnome-terminal
# but we chose xterm
TERMCMD = "${XTERM_TERMCMD}"
TERMCMDRUN = "${XTERM_TERMCMDRUN}"
# Don't generate the mirror tarball for SCM repos, the snapshot is enough
BB_GENERATE_MIRROR_TARBALLS = "0"
# Uncomment this to remove work directory after packaging to save disk space
#INHERIT += "rm_work"
# Keep one set of images by default
RM_OLD_IMAGE = "1"
# Enable local PR service for binary feeds
PRSERV_HOST = "localhost:0"
# It is recommended to activate "buildhistory" for testing the PR service
INHERIT += "buildhistory"
BUILDHISTORY_COMMIT = "1"