Hi TI support team,
I'm working on AM335x. I want header file for AM335x. Plaese tell me where can I get source code?
Thanks,
Regards,
Priyadharshini M.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi TI support team,
I'm working on AM335x. I want header file for AM335x. Plaese tell me where can I get source code?
Thanks,
Regards,
Priyadharshini M.
Hi Priyadharshini,
Have you tried to download the AM335x Processor SDK from the link below?
Building the SDK:
Also, what header file in general are you looking for in the source code?
Best Regards
Suren
Hi suran,
Thanks for replying to me.
I've already downloaded the SDK from this link below.
And I installed SDK using the link provided below.
I'm also downloading CC Studio from the link below.
I'd like to begin with a simple programme for GPIO pins (High and Low).Please kindly guide me on how to create an AM3359 project on CC, which header files are needed, and if header files are needed, please guide me to where I can download and include them.
Please reply to me as soon as possible.
Thanks,
Regards,
Priyadharshini M
Hi Priyadharshini,
I am assigning your query to our expert in CCS with AM335x. You should be receiving a response soon.
Best Regards,
Suren
Hi Priyadharshini,
I'd like to begin with a simple programme for GPIO pins (High and Low).Please kindly guide me on how to create an AM3359 project on CC, which header files are needed, and if header files are needed, please guide me to where I can download and include them.
Just to clarify, is your program to run in Linux or bare-metal?
Thanks,
Jianzhong
Hello Jianzhong,
I'm very new to this field. Please explain the difference between running a programme in Linux and running it on bare metal.
Thanks,
Priyadharshini
Hi Priyadharshini,
Are you planning to run Linux on your AM335x board and access GPIO within Linux, or writing a simple program without using Linux?
Thanks,
Jianzhong
Hi Jianzhong ,
I want to write a simple GPIO programme on CSS and load it onto the AM335x ICE Board.
Please guide me on how to create a project, what header files the project needs, and how to load that programme on the AM335x ICE Board.
Thanks,
Priyadharshini M
Ok. Please refer to the AM335x TI-RTOS/bare-metal development resource, especially:
Getting started with RTOS or Bare-metal Development:
Regards,
Jianzhong
Hi Jianzhong,
I'm planning to run linux on my AM3359ICE board and access GPIO within LInux.
please guide me how to create and run.
Thanks in advance.
Regards,
Priyadharshini
Hi Jianzhong,
I'm working on an RTOS Baremetal project with the link you've already provided.
https://e2e.ti.com/support/processors-group/processors/f/791/t/104447
I built and loaded the project successfully when I imported it directly.
However, I encountered some issues while attempting to build the project on my own using your instructions from another post.
https://e2e.ti.com/support/processors-group/processors/f/791/t/1044470
please tell me how to resolve these errors.
Regards,
Priyadharshini
Hello Priyadharshini,
Please try to compare the compiler settings between the two CCS projects: the one you downaloded and the one you created on your own.
Regards,
Jianzhong
Hi Jianzhong,
Thanks for your help.
I'm sucessfully loaded the led blink program which you provided. please tell me how to reconstruct the program. because I got no response when i modify the userled0 and 1. on board only four leds directly connected to the board.
LED1--GPIO0_17
LED2--GPIO3_1
LED3--GPIO0_29
LED4--GPIO1_30
please tell me how to toggle these four LEDs.