The "Eth & EthTrcv User Guide" partition of the drv_docs contained in the MCAL_AM62x_00.09.00.02 mentions that the DMA interrupt numbers can be set via configuration parameters dmaTxChIntrNum and dmaRxChIntrNum. The valid interrupt numbers depend on the SOC's resource allocation. For AM62x the starting resource is supposed to be DMASS0_INTAGGR_0_INTAGGR_VINTR_PEND_44 which is nowhere to be found in the TRM („Literature Number: SPRUIV7A., MAY 2022 – REVISED NOVEMBER 2022.“).
Is this information missing in the TRM or might this be some inconsistency between MCAL documentation and TRM?