This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Using 4-bit ECC AM3517 EVM

Hi,

I'm not having any luck getting x-load to load u-boot using 4-bit ECC.

I have built x-load with the FOUR_BIT_ERROR_CORRECT define set and when using u-boot (booted from MMC) to write the NAND I have selected "nandecc bch4_sw".

But I am getting:

Texas Instruments X-Loader 1.51 (Jun 29 2011 - 13:09:45)                        

Booting from nand . . .                                                         

Error: Bad compare! failed                                                      

ECC Failed, page 0x00080000

So I left x-load as is and flashed uImage using the five different options (from Minicom):

#send "nandecc bch4_sw" 

#send "nandecc hw 2"  

#send "nandecc bch8_sw" 

#send "nandecc hw 1" 

send "nandecc sw 1" 

They all produced the same results.

While I am on the subject: I find this option confusing. My understanding is that the GPMC can detect 1/4/8 bits but not correct them. May I interpret the options in the following way?

bch4_sw: The GPMC will detect errors in 4-bit mode and if detected the driver will use BCH to correct.

bch8_sw: Similar to above except 8-bit.

hw1/hw2: Some message about x-load/u-boot versus kernel/filesystem that makes no sense in this context.

sw1: The GPMC will detect errors in 1-bit mode and if detected the driver will attempt to correct.

Is it possible to have detection only with no correction?

Thanks,

Ken