This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MCBSP driver provided with kernel 2.6.37 does not work on OMAP L138 EVM

Hi,

 

I am using kernel 2.6.37 (part of DaVinci-PSP-SDK-03.21.00.04) on OMAP L138 EVM board.

The kernel has mcbsp driver(under arch/arm/mach-davinci/mcbsp.c). The PSP has a example application for it, in the form of a loadable module.

I do not have 2 EVM's to connect their MCBSP to test, as recomended in the application note.

However I am trying use the example to transmit packets in master mode using following command:

"insmod mcbsp_test.ko num_pkts=5 master=1 tx_rx=1"

 

I expected to see transmitted data on Ocilloscope.

But when I insert the module I see "BCLK" starts(~2.7MHz) but I do not see activity on any other lines(DOUT, WCLK).

Is there some issue with the MCBSP driver ?  Anyone seen such issue ?

 

Thanks,

Snehal