Hi all,
I want to learn about ISP configuration on DM355.I have the following doubts.
1.Is there any tutorial or document which explains about ISP configuration or ISP basics on DM355/DM365.
2.If we need to write separate drivers for configuring ISP and insert those in kernel and then have to call apis in drivers from application or there
is any other way to do that.
3.To realize the optimum performance of DM355/DM365 camera other than ISP configuration if we can do any other thing to improve image quality.
Thanks and Regards,
Mayank