Hi,
We are using Davinci DM6467 in our design, the processor used is TMS320DM6467ZUTA. DVSDK that we are using for our application is dvsdk_2_00_00_22 and the TI Kernel Version is linux-2.6.18_pro500. I have query on McASP0 interface, we want to use McASP0 serializer 2 in receive mode to analyze the data’s.for configuring serialiser 2 as Rx mode i changed the
static u8 dm646x_iis_serializer_direction[] = {
TX_MODE, RX_MODE, RX_MODE, INACTIVE_MODE,
}; in Davince-evm.c
but i could not read the data in serialiser 2 ,could any one can tell me what are the other changes i need to do for configuring serializer0 as Tx mode,serialiser1 as Rx mode and serialiser2 as Rx mode so that i could read the data in serialiser 1 and serialiser 2 induvidually.
Regards
Parthipan