This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA4VM: It was stuck when the model was being converted

Part Number: TDA4VM

Hi Team,

ti-processor-sdk-rtos-j721e-evm-07_03_00_17+ tidl_j7_02_00_00_07

One of the two onnx files with the same structure and yet different network parameters can complete the conversion normally, and the other one gets stuck and reports a Segmentation fault (core dumped) before the end of the first Calibration iteration. I notice that the T values of the image output of the two models are very different during the conversion. What do these T values mean? Are they the cause of the fault?

Kind regards,

Katherine