Part Number: AM62X-PET-CALC
Hi TI
In the power estimation tool, how to selec the mode column list as below?what's the represent meaning of every item?when i used this port as GPIO which one can i select?

BR JINGCHENG
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: AM62X-PET-CALC
Hi TI
In the power estimation tool, how to selec the mode column list as below?what's the represent meaning of every item?when i used this port as GPIO which one can i select?

BR JINGCHENG
Hi Jingcheng,
The '<X>_<Y>' of the modes fields that you circled for UART are:
x = baud rate
y = TTL voltage level, i.e 3.3 or 1.8V
Regards,
Colin
Hi Colin
When configreate as GPIO , which mode can be select? and how to eccess the IO Utilization when used as GPIO?
BR Jingcheng
HI Colin
For UART, I only used the RX/TX two pins , CTS/RTS is not used, So the IO utilization is 50% ? is it correct?
BR Jingcheng
Hi Jingcheng,
if you are using the UARTs constantly without stopping then 100% would be appropriate. If you are using the peripheral one out of 10 minutes, then 10% would be appropriate.
The %Utilization that you choose should be an estimate based on how often the peripheral is used.
Regards,
Colin