This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA4VM-Q1: Use case power estimation for PMIC capacity analysis

Part Number: TDA4VM-Q1

I have a question according to the power estimation which you provided for the attached use case:
Is it possible to get more detailed information about the distribution of power to the supply rails?
We plan to design the supply topology for TDA4VM88T according to SLVUC99A (PDN-0C) and have to calculate/verify if the recommended components (PMIC/Buck/Switch) are suitable for the use case mentioned above

Regards, Peter

Core Frequency [MHz] Activity (0% to 100%)
Processors
ARM A72 Processor 2000 100
ARM A72 Processor 2000 100
ARM R5F (x2) 1000 100
ARM R5F (x2) 1000 100
C66x DSP 1350 0
C66x DSP 1350 0
C711 DSP 1000 0
Matrix Multiply Accelerator 1000 0
WKUP/MCU
Device Management Security Controller 333 5
ARM R5F (x2) -- for safety monitor, often used in Lock-step 1000 100
Multimedia and HWA
Display Sub-System; Embedded Display Port; MIPI Display Serial Interface 600 0
Graphics Processing Unit (up to 96GFlops) 750 0
Camera Streaming Interface 720 0
Depth and Motion Processing Accelerator 520 0
Vision Processing Accelerator 720 0
Video Decoder (up to 4K/60) 550 0
Video Encoder (up to 1080p/60) 700 0
High Speed Serial Interface Controllers
9-port Gigabit Ethernet Switch 320 50
Industrial Communication Subsystem - Gigabit 275 0
Industrial Communication Subsystem - Gigabit 275 0
PCIe (Peripheral Component Interconnect Express) 500 100
PCIe (Peripheral Component Interconnect Express) 500 100
PCIe (Peripheral Component Interconnect Express) 500 100
PCIe (Peripheral Component Interconnect Express) 500 0
Universal Flash Storage Host Controller Interface 250 0
USB3.1 Gen 1 (Universal Serial Bus) 312,5 0
USB3.1 Gen 1 (Universal Serial Bus) 312,5 0
Memory Interfaces
Low Power DDR4 2132 100
Interfaces
SerDes - 2L   ON
SerDes - 2L   ON
SerDes - 2L   ON
SerDes - 2L   OFF
SerDes - 4L   OFF
DPHY 1.2 RX - 4L   OFF
DPHY 1.2 RX - 4L   OFF
DPHY 1.2 RX - 4L   OFF
DPHY 1.2 RX - 4L   OFF
MPHY - 2L   OFF
LPDDR4 32b inline ECC 4267   ON
eMMC   OFF