This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Setting up boundary scan for AM3505

Other Parts Discussed in Thread: AM3505

I'm trying to connect an AM3505 to XJTAG. I have established a JTAG chain but when I load the bsdl file into XJTAG to compare with the ARM microprocessor, it doesn't match. I have had a look at all the points in the chain and they are working fine. Also, in the bsdl file, the compliance_pattern nets are all in the high state when measured. The image shows the bsdl file loaded into the library properly but when it reads the chain, it returns the status of No BSDL matches found. Can anybody please give some suggestions? Thanks, Matt