Part Number: AM3359
I've downloaded SDK from below link,
when I run ./setup.sh, I got
priyadharshini@priyadharshini-HP-280-G4-MT-Business-PC:~/ti-processor-sdk-linux-am335x-evm-08.02.00.24$ ./setup.sh
-------------------------------------------------------------------------------
TISDK setup script
This script will set up your development host for SDK development.
Parts of this script require administrator priviliges (sudo access).
-------------------------------------------------------------------------------
--------------------------------------------------------------------------------
Verifying Linux host distribution
Ubuntu 18.04 LTS is being used, continuing..
--------------------------------------------------------------------------------
Starting with Ubuntu 12.04 serial devices are only accessible by members of the 'dialout' group.
A user must be apart of this group to have the proper permissions to access a serial device.
User 'priyadharshini' is already apart of the 'dialout' group
-------------------------------------------------------------------------------
setup package script
This script will make sure you have the proper host support packages installed
This script requires administrator priviliges (sudo access) if packages are to be installed.
-------------------------------------------------------------------------------
System has required packages!
--------------------------------------------------------------------------------
Package verification and installation successfully completed
--------------------------------------------------------------------------------
--------------------------------------------------------------------------------
In which directory do you want to install the target filesystem?(if this directory does not exist it will be created)
[ /home/priyadharshini/ti-processor-sdk-linux-am335x-evm-08.02.00.24/targetNFS ]
--------------------------------------------------------------------------------
--------------------------------------------------------------------------------
This step will extract the target filesystem to /home/priyadharshini/ti-processor-sdk-linux-am335x-evm-08.02.00.24/targetNFS
Note! This command requires you to have administrator priviliges (sudo access)
on your host.
Press return to continue
Multiple filesystems found.
1:tisdk-default-image-am335x-evm.tar.xz
2:tisdk-docker-rootfs-image-am335x-evm.tar.xz
Enter Number of rootfs Tarball: [1 or 2] 1
[sudo] password for priyadharshini:
Successfully extracted tisdk-default-image-am335x-evm.tar.xz to /home/priyadharshini/ti-processor-sdk-linux-am335x-evm-08.02.00.24/targetNFS
--------------------------------------------------------------------------------
--------------------------------------------------------------------------------
This step will set up the SDK to install binaries in to:
/home/priyadharshini/ti-processor-sdk-linux-am335x-evm-08.02.00.24/targetNFS/home/root/am335x-evm
The files will be available from /home/root/am335x-evm on the target.
This setting can be changed later by editing Rules.make and changing the
EXEC_DIR or DESTDIR variable (depending on your SDK).
Press return to continueRules.make edited successfully..
--------------------------------------------------------------------------------
--------------------------------------------------------------------------------
This step will export your target filesystem for NFS access.
Note! This command requires you to have administrator priviliges (sudo access)
on your host.
Press return to continue/home/priyadharshini/ti-processor-sdk-linux-am335x-evm-08.02.00.24/targetNFS already NFS exported, skipping..
[ ok ] Stopping nfs-kernel-server (via systemctl): nfs-kernel-server.service.
[....] Starting nfs-kernel-server (via systemctl): nfs-kernel-server.serviceJob for nfs-server.service canceled.
failed!
Failed setup, aborting..
Failed setup, aborting..
priyadharshini@priyadharshini-HP-280-G4-MT-Business-PC:~/ti-processor-sdk-linux-am335x-evm-08.02.00.24$
Please tell me what error I got and how to resolve it.
Thanks & Regards,
Priyadharshini.