This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Clarification about cmem, dsplink and linux memory



I have a project on an omap L138 board, but I have a few question about memory map.

In a project using dsplink only, what can I do with the cmem memory ?

Linux uses 64 meg of DDR,  from c0000000 to c4000000. If my memory map
starts at c3e00000, then evrything is fine. However, if I put it at c4000000, then
my program hangs when calling procload.

Precision :
I modified the memory map both on the GPP and the DSP side.

When using dsplink only, should the memory used by GPP + DSP be
inside the region mapped by the kernel ?

What can I do with the cmem memory when not using codec engine ?

 

  • It is working after a reset of the board.

  • Is there any constraint regarding the size of the DDR segment allocated in the DSP memory map ?
    In the following table, if I set CODEMEMORY size to 0xFFFF80 instead of 0xFFF80, then my
    test application either

    - hangs in procLoad
    - crash the board (kernel panic)
    - hangs the board

    the tcf file is modified accordingly.

    Is there any constraints for the distance between the start of the code section, and the start of the
    shared memory section holding the dsplink objetcs ?

     

    /** ============================================================================
     *  @name   LINKCFG_memTable_00
     *
     *  @desc   Memory table ID 0.
     *  ============================================================================
     */
    STATIC LINKCFG_MemEntry  LINKCFG_memTable_00 [] =
    {
        {
            RSTENTRYID,                        /* ENTRY          : Entry number */
            "RESETCTRL",                       /* NAME           : Name of the memory region */
            RESETCTRLADDR,                     /* ADDRPHYS       : Physical address */
            RESETCTRLADDR,                     /* ADDRDSPVIRT    : DSP virtual address */
            (Uint32) -1,                       /* ADDRGPPVIRT    : GPP virtual address (if known) */
            RESETCTRLSIZE,                     /* SIZE           : Size of the memory region */
            FALSE,                             /* SHARED         : Shared access memory? */
            FALSE,                             /* SYNCD          : Synchornized? */
        },
        {
            CODEENTRYID,                       /* ENTRY          : Entry number */
            "DDR",                             /* NAME           : Name of the memory region */
            CODEMEMORYADDR,                    /* ADDRPHYS       : Physical address */
            CODEMEMORYADDR,                    /* ADDRDSPVIRT    : DSP virtual address */
            (Uint32) -1,                       /* ADDRGPPVIRT    : GPP virtual address (if known) */
            CODEMEMORYSIZE,                    /* SIZE           : Size of the memory region */
            FALSE,                             /* SHARED         : Shared access memory? */
            FALSE,                             /* SYNCD          : Synchornized? */
        },
        {
            SHAREDENTRYID0,                   /* ENTRY          : Entry number */
            "DSPLINKMEM",                     /* NAME           : Name of the memory region */
            SHAREDMEMORYADDR0,                /* ADDRPHYS       : Physical address */
            SHAREDMEMORYADDR0,                /* ADDRDSPVIRT    : DSP virtual address */
           (Uint32) -1,                      /* ADDRGPPVIRT    : GPP virtual address (if known) */
            SHAREDMEMORYSIZE0,                /* SIZE           : Size of the memory region */
            TRUE,                             /* SHARED         : Shared access memory? */
            FALSE,                            /* SYNCD          : Synchornized? */
        },
        {
            SHAREDENTRYID1,                   /* ENTRY          : Entry number */
            "DSPLINKMEM1",                     /* NAME           : Name of the memory region */
            SHAREDMEMORYADDR1,                /* ADDRPHYS       : Physical address */
            SHAREDMEMORYADDR1,                /* ADDRDSPVIRT    : DSP virtual address */
            (Uint32) -1,                      /* ADDRGPPVIRT    : GPP virtual address (if known) */
            SHAREDMEMORYSIZE1,                /* SIZE           : Size of the memory region */
            TRUE,                             /* SHARED         : Shared access memory? */
            FALSE,                            /* SYNCD          : Synchornized? */
        },
        {
            POOLENTRYID,                       /* ENTRY          : Entry number */
            "POOLMEM",                         /* NAME           : Name of the memory region */
            POOLMEMORYADDR,                    /* ADDRPHYS       : Physical address */
            POOLMEMORYADDR,                    /* ADDRDSPVIRT    : DSP virtual address */
            (Uint32) -1,                       /* ADDRGPPVIRT    : GPP virtual address (if known) */
            POOLMEMORYSIZE,                    /* SIZE           : Size of the memory region */
            TRUE,                              /* SHARED         : Shared access memory? Logically */
            FALSE,                             /* SYNCD          : Synchornized? */
        },
        {
            5,                     /* ENTRY          : Entry number */
            "DSPIRAM",             /* NAME           : Name of the memory region */
            0x11800000,            /* ADDRPHYS       : Physical address */
            0x11800000,            /* ADDRDSPVIRT    : DSP virtual address */
            (Uint32) -1,           /* ADDRGPPVIRT    : GPP virtual address (if known) */
            0x40000,               /* SIZE           : Size of the memory region */
            FALSE,                 /* SHARED         : Shared access memory? */
            FALSE,                 /* SYNCD          : Synchornized? */
        },
        {
            6,                     /* ENTRY          : Entry number */
            "DSPL1DRAM",           /* NAME           : Name of the memory region */
            0x11F00000,            /* ADDRPHYS       : Physical address */
            0x11F00000,            /* ADDRDSPVIRT    : DSP virtual address */
            (Uint32) -1,           /* ADDRGPPVIRT    : GPP virtual address (if known) */
            0x8000,                /* SIZE           : Size of the memory region */
            FALSE,                 /* SHARED         : Shared access memory? */
            FALSE,                 /* SYNCD          : Synchornized? */
        },
    } ;