I tried to run the example in CSL_MMCSD_SdCardFSExample and got the following failure :
MMCSD-ATAFS TESTS!
MMCSD-ATAFS POLL MODE TEST!
SD Card detected
SD card is High Capacity Card
Memory Access will use Block Addressing
SD card initialization Successful
ATA File System Initialization successful
ATA_fileInit error (0x300)
I am using CSL version 2.10.00.00 on a 5515eZDSP board and a microSD card with 4GB formtted to FAT(32) with 4096 block size
The same setup is passing a test without a file system in CSL_MMCSD_SdCardExample
While tracking the failure I saw that it fails in ATA_Cdroot function
Can anyone hint about the reason for the failure ?
Thanks
Zeev