Part Number: TDA4VM
In datasheet, pin A23/E22 are defined as MCU_OSPI0_RESET_OUT pins in OSPI0 bus.
Is it possible to implement the MCU_OSPI0_RESET_OUT function via a regular GPIO, while free A23/E22 for their secondary functions, e.g. MCU_OSPI1_CSn1 (E22), MCU_OSPI1_LBCLKO (A23)..
what's the special of these embedded OSPI reset pins? What's the concerns/risk/tradeoff (software effort) if the OSPI reset function is implemented by a regular GPIO?
The reason I am asking is in our design, OSPI1 (we just use as a standard SPI) required two CS signals, but one supported pin E22 has been used as MCU_OSPI0_RESET_OUT1 by OSPI0. To minimize the pinout shuffle to relocate this SPI, we would like to see the feasibility of above proposal.
Thanks!