Other Parts Discussed in Thread: OMAP-L138
Hello,
I am developing a Qt application on omap-l138. This application use a library previously built with c6runLib. When I call a function from this library, I'd like to pass a pointer to a structure (allocate on ARM side) as a parameter, but it seems that the adress is different on DSP side than on ARM side.
I tried to allocate a structure in a C program om ARM side and passed it through a function parameter and it is actually working. So I guess that malloc( ) function from C lib allocates in shared memory, which is not the case with malloc from c++ lib.
So my questions are:
1) What is the difference between C++ and C allocation?
2) How can I specify the memory allocation to be done in shared memory?
3) Is there any c6runlib example using shared memory?
Thanks in advance