This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Has Timer changeed in 6678 compared with 6455?

Hello:

    since there is no document about 64 bit timer for keystone 66x,I wonder whether the timer is the same with c6455?can I use the program that fits  c6455 into 6678?

  thanks

  • The Keystone Timer User's Guide should be completed soon but until it is available you can refer to the C6457 Timer User's Guide.  It uses the same timer subsystem as the C6678 and should closely resemble the Keystone Timer User's Guide once it is complete.