Other Parts Discussed in Thread: CCSTUDIO
Necessary to combine two of the project audioSample.pjt and mmcsdSample.pjt. The problem is the following. On the SD card has a wave file format. In memory of DSP is allocated a large buffer, then in an endless loop sequence reads this file to the allocated buffer and play it through the audio codec. The operation of reading a file from the SD card is successful, the function playing SIO_reclaim hangs in an endless waiting for an empty buffer. I have such expectations, it is associated with the use of channels edma3. Example code:
use:
1. CCStudio_v3.3
2. bios_5_41_00_06
3. pspdrivers_01_30_00_06
3. rtfs_1_10_02_32
Thanks