This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Supported NAND Devices



The DM816x/C6A816x/AM389x device ROM supports the NAND devices with the IDs in the table below.   In addition, ROM code also supports NAND devices which are ONFI compliant.  If a NAND device doesn't fall in the below list and is not ONFI compliant, it can still be supported by having the NAND parameters in an I2C EEPROM.

Supported NAND Devices


Capacity

Device ID

Bus Width

Page size

512 Mb

F0

x8

2048

512 Mb

C0

x16

2048

512 Mb

A0

x8

2048

512 Mb

B0

x16

2048

512 Mb

F2

x8

2048

512 Mb

C2

x16

2048

512 Mb

A2

x8

2048

512 Mb

B2

x16

2048

1 Gb

F1

x8

2048

1 Gb

C1

x16

2048

1 Gb

A1

x8

2048

1 Gb

B1

x16

2048

2 Gb

DA

x8

2048

2 Gb

CA

x16

2048

2 Gb

AA

x8

2048

2 Gb

BA

x16

2048

2 Gb

83

x8

2048

2 Gb

93

x16

2048

4 Gb

DC

x8

2048

4 Gb

CC

x16

2048

4 Gb

AC

x8

2048/4096

4 Gb

BC

x16

2048/4096

4 Gb

84

x8

2048

4 Gb

94

x16

2048

8 Gb

D3

x8

2048/4096

8 Gb

C3

x16

2048/4096

8 Gb

A3

x8

2048/4096

8 Gb

B3

x16

2048/4096

8 Gb

85

x8

2048

8 Gb

95

x16

2048

16 Gb

D5

x8

2048/4096

16 Gb

C5

x16

2048/4096

16 Gb

A5

x8

2048/4096

16 Gb

B5

x16

2048/4096

16 Gb

86

x8

2048

16 Gb

96

x16

2048

32 Gb

D7

x8

2048/4096

32 Gb

C7

x16

2048/4096

32 Gb

A7

x8

2048/4096

32 Gb

B7

x16

2048/4096

32 Gb

87

x8

2048

32 Gb

97

x16

2048

64 Gb

DE

x8

2048/4096

64 Gb

CE

x16

2048/4096

64 Gb

AE

x8

2048/4096

64 Gb

BE

x16

2048/4096