This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCSTUDIO: GUI Composer Refresh Rate

Part Number: CCSTUDIO

Hi,

What is the maximum refresh rate of the GUI composer ? Can I plot the graph with 100Hz ? 

Thanks

  • Hello,

    There are several factors to take into account, such as the transport used, how the data is buffered, and the type of GC solution.

    100Hz is quite fast and I would recommend buffering the data on the target and then sending it out in larger chunks so that GC does not have to refresh as often.

    Thanks

    ki