Hi TI experts
I am using the camera sensor which the format of the data output is RAW12, but in the sensor driver, the “tivx_raw_image_format_t” in “IssSensor_CreateParams” struct should be {TIVX_RAW_IMAGE_16_BIT, 11}, and I try to change it to "TIVX_RAW_IMAGE_P12_BIT", but it can't output the image normally.
So I want to know the reason ,why I shoud choose "{TIVX_RAW_IMAGE_16_BIT, 11}" in the driver, despite the sensor I used is RAW12 output.

For more infomation, I am using QNX and RTOS in SDK8.2.
I'm looking forward to your replay.