hello,
I am trying to test VLAN with the EST function of TSN,but I found that when I connecting a VM board with a VH board, the configured ETH0.100 can send a message with VLAN, but it can not receive the message with 100 VID on the VM end.
I have used the following instructions to add a virtual network card for VLAN100 on both ends
ip link add link eth0 name eth0.100 type vlan id 100