This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRA829V-Q1: Quality Questions

Part Number: DRA829V-Q1

Can TI offer this part as an EP (-55 °C) part?

Can we obtain this part with a tin-lead ball?

In general, what is underneath the lid?

Are there any pure tin components under the lid?

Is the lid vented; if so, how?

What type of SAC ball is used (305, 405)?

In the photo below, what are the four components shown in the BGA?

Are the components attached with a high-temp solder?

Will the components come off if we attempt to reball or use a longer dwell time for using the SAC?