Hello,
i have a customer that wants to develop a video application, where DN365 or DM368 could fit, The customer wants to encode using H.264 and D1 resolution but would need a bit rate of 1Mbps or 2Mbps maximun. Customer has downloaded documentation for H.264 encoding in DM36x, but does not find if DM36x can achieve this bit-rate for D1 and H.264 specs. Pls. could you help me with this subject?
Many thanks