Part Number: AM3358
Other Parts Discussed in Thread: AM4379
I downloaded ti-processor-sdk-linux-am335x-evm-08.02.00.24-Linux-x86-Install.bin and installed it on a Ubuntu 18.04 system (running in a VirtualBox VM). I attempted to generate for a Beaglebone Black. I followed the online instructions but when I get to the step that would recognize the Beaglebone, the Beaglebone is not recognized. I examined the install script and the USB signature it is looking for is not present. I looked at the USB signature on the host machine and it does appear there either.
I would appreciate any advice you can provide.
PS. I ultimately want to develop a Linux for the AM5379 which I am implementing in a new design. The Linux for the AM3358 was intended as a first step to generate for a known working target machine. If an existing Linux implementation exists for either of these processors that I could learn from, I would appreciate that information.