This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

aic23 problem

i have a problem with utilizing the DAC and ADC (AIC23 IC INTEGRATED ON THE KIT ) on the C6455 DSK , now i am able to send a voice signal and hear it back from the kit and process it too , but i need to hear the voice for certain time and stop the  aic23 for some time and hear it again after that

where exactly the place in the code , that i can perform this task ?

3157.dsk_app.rar

 

attached the c file for the dsk_app

thanks in advance

  • Ahmed,

          Why do you need to stop the AIC23? This is a very atypical use case.

     If you can narrow the scope of your question, we can potentially point to a corresponding resource, however since the project you have included is not complete, there is little assistance we can provide you with.

    I would recommend you read through the source code to determine where the data is being transmitted from the C6455 to the AIC23.