This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA4VM: MSMC Resource Arbitration

Part Number: TDA4VM

Hi,

In the TDA4VM TRM 8.1.3.6, may I confirm that the same endpoint of MSMC just means the same address of RAM?

Kind Regards,

Kevin

  • Hi Kevin,

    Please reference TRM 3.3 System Interconnect Functional Description, for further information on the term 'endpoint'.   

    The device is comprised of multiple modules connected together by "interconnects".    Each module is a classified as an "Initiator" or "Target/Destination" ... (Master / Slave).   Each "target/destination" is an endpoint in the snippet pasted above from TDA4VM TRM 8.1.3.6.   

    In the example given of "same RAM address", yes they would be routed the same endpoint.   Two different addresses may also be routed targeting the same endpoint.

    Regards,

    kb