Hi,
My customer wants to evaluate thermal behavior using SK-AM62.
He wants to read VTM temp sensor value from Linux SDK console.
Please tell me how to get the sensor value using console command?
Thanks and regards,
Koichiro Tashiro
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
My customer wants to evaluate thermal behavior using SK-AM62.
He wants to read VTM temp sensor value from Linux SDK console.
Please tell me how to get the sensor value using console command?
Thanks and regards,
Koichiro Tashiro
Hi Bin,
The customer tried the command, but it does not work.
Here is the log output.
root@am62xx-evm:~# cat /sys/class/thermal/thermal_zone1/temp cat: /sys/class/thermal/thermal_zone1/temp: No such file or directory root@am62xx-evm:~# root@am62xx-evm:~# root@am62xx-evm:~# root@am62xx-evm:~# cat /sys/class/thermal/thermal_zone*/temp cat: '/sys/class/thermal/thermal_zone*/temp': No such file or directory root@am62xx-evm:~# cd /sys root@am62xx-evm:/sys# ls block bus class dev devices firmware fs kernel module power root@am62xx-evm:/sys# cd /class -sh: cd: /class: No such file or directory root@am62xx-evm:/sys# cd class root@am62xx-evm:/sys/class# cd thermal/ root@am62xx-evm:/sys/class/thermal# ls root@am62xx-evm:/sys/class/thermal# ls root@am62xx-evm:/sys/class/thermal#
Hi Tashiro-san,
I just reviewed the kernel source code, I think you need to use at least SDK v8.4. Please try with the following SDK v8.5 SD card image:
I am not sure if E1 SK is still supported in SDK8.5. So if the above image doesn't boot, please try the following SDK8.4 SD card image: