This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA4VM: Question of mipi protocol and Virtual Channels

Part Number: TDA4VM

I have a question regarding the mipi protocol and virtual channels:

Is the mipi Hard Ip Core in the TDA4 capable of doing the following communication?
The figure shows a mipi stream which I copied from the mipi spec. It is named as "Interleaved Video Data Streams". It does not show the typical FS FE short packages which are recommended for Interleaved Video streams in a later chapter. Nevertheless, will the TDA4 understand the below streaming without FS/FE? 
M understanding is that in the Packet Header the Data Type ID can be the same and the virtual channel has 0 or 1 as described in the picture.
Thank you!
Highway