Other Parts Discussed in Thread: DM3730
Hi,
My customer is working on a MACHINE VISION Project.
They are working with DM3730 processor through BeagleBoard-XM . The interfacing of Aptina MT9P031 with BeagleBoard-XM was done successfully.
They are using Angstrom Linux on BeagleBoard-XM with kernel 2.6.32 which includes V4L2 drivers. They have been successful in capturing an image & process it in their C code.
But the Aptina MT9P031 is not fully suitable for their project. They plan to use the Aptina-MT9V032 in this Project.
They have tried to interface Aptina-MT9V032 with existing V4L2 drivers but did not get the image. Think the drivers are not compatible with Aptina-MT9V032.
Can you help with the below -
1)Send us driver for Aptina-MT9V032 .
2)Guide to make existing drivers (Aptina-MT9P031) compatible for Aptina-MT9V032.
Awaiting your reply.
Thanks
Suman G.