Whether AM3517 can boot from SPI flash???
when set SYS.BOOT[5:0]=0b111100 that means the boot sequence is UART SPI,the AM3517 can't work correctly,
because there are no signals output on SPI1 pins and also no uart output at all.
so why?
-------------------------------------------
If can boot AM3517 from SPI flash,which SPI port should be used? the AM3517 has four SPI PORT[1-4].
Does the spi flash sector size must be 512bytes?
Does the flash tool supports SPI download in futures?
---------------------------------------------
Best Regards.