Hi, everyone
Let me tell you guys what i am using first,
CCSv5.0.2.00006
OMAP3530 beagleboard.
xds100v2 emulator
Windows xp/windows 7
Note: i am not using any of the linux based applications.
I had mp3 decoder code for c64x+ CPU which i had successfully debugged and tested usng the CCSv5 and DSP/BIOS 5 okay.
Now my next task is that i want to move to the CCSv5 and SYS/BIOS (BIOS 6), where i know that there is difference between SYS/BIOS and DSP/BIOS. I tried somewhat for it, but seems that i am lost somewhere while modifying the codes and changing the paths defined. I had gone trough the migration guide form BIOS 5 to BIOS 6, but there isn't much data available. There are some files which are not available in the BIOS6 with respect to the BIOS 5. I tried contact some person and i came to know that PSP packages and some drivers are still in development level for Linux based and BIOS based driver.
Can any one over here tried project like this. I mean changing the some project to BIOS 6 from BIOS 5 based. If any one interested then i am attaching my current project. someone can have look and suggest me what to do next.
I knew, it will be great learning platform while working on this project since we need to have complete understanding of the BIOS 5 as well as BIOS 6 up to each file level.
With Regards
Nitin Mewada