Other Parts Discussed in Thread: CCSTUDIO
I am trying to build the biosusb device MSC example project for the EVM6747.
When I compile the bios usbdevmsc.tcf I get the following message.
[usbdevmsc.tcf] "C:\CCStudio_v3.3\bios_5_41_10_36\xdctools\tconf" -b -Dconfig.importPath="C:/CCStudio_v3.3/bios_5_41_10_36/packages" usbdevmsc.tcf
js: "./usbdevmsc.tcf", line 174: Failed to generate config files.
Compile Complete,
1 Errors, 0 Warnings, 0 Remarks.
line 174 of the .tcf file is prog.gen();
I am using CCS3.3 ver 3.3.82.13. I have tried with DSP/Bios 5.33.04 and 5.41.10.36 and get the same message.
USB driver installation: C:\Program Files\Texas Instruments\biosusb_01_00_00\packages\ti\biosusb\examples\usbdevmsc\build\usbdevmsc.tcf
I have several other Bios .tcf files that compile correctly.
any hints in what causes this error message?
Thanks