Other Parts Discussed in Thread: TDA4VH
Hello,
I could boot the VH board with SDK 8.2.2.
But I could not boot the board with SDK 8.5.
I followed the same instructions.
Is there something else I need to do?
Best regards,
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello KB,
I am using these; 08.05.00.XX
https://www.ti.com/tool/download/PROCESSOR-SDK-LINUX-J721E/08.05.00.08
https://www.ti.com/tool/download/PROCESSOR-SDK-RTOS-J721E/08.05.00.11
I used microSD card booting mode(I could boot with a microSD card with 8.2.2, and I did not change a boot mode)
I could see 4 serial ports active /dev/ttyUSBX.
There is no serial output from the board.(I could see the booting log with 8.2.2)
Best regards,
Hello
It could be because of the uploaded TI SDK.
Its name is ti-processor…j721e-evm…tar.gz, which is not VH
It should be like the file name: ti-processor…j784s4…tar.gz
How to configure the SDK for VH, and where can I download the bootloader and rootfs for VH?
Best regards,
Hi,
You will need to use the SDK corresponding to TDA4VH.
The release should be available before the end of the week at this location: https://www.ti.com/product/TDA4VH-Q1#software-development
Kindly try to prepare a new SD card by following the procedure. If the problem persists, please come back on this thread.
Regards
Karthik