Other Parts Discussed in Thread: OMAP3530
I am facing a weird situation with an Omap3530 EVM running WinCE 6.0. WinCE works fine as I attach my device to Visual Studio 2005 that downloads the image to the device and then WinCE 6.0 is running (I have also activated the kernel debugger option).
Now, I have an application from an other project and I want to make it work on this board. It was created in Visual Studio 2008. I have managed to compile it using the SDK from my BSP, so, I expect that if I download the program to the WinCE 6.0 that are running using the VS 2005, it will run without problems.
My question is can I attach the device on both Visual Studios through Ethernet? (I tried but it didn't work)
Is there any other way?
Thank you!