This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LP-AM263: LP-AM263

Part Number: LP-AM263


Hello,

I'm playing with mcan_external_read_write. I can transmit message from launchpad and sniff it via Vehicle SPY. The following picture represents console log after transmission.

Here application is waiting for incoming mcan messages. And after I can receive message, which was sent from Vehicle SPY.

The first Tx/Rx cicle is working. But when I am going to do it at the second time. The board is sitting in the hardware interrupt and do nothing. After running the application in the console I have this

When I am click pause it he debugger, I have this:

I am also tried to reset MCAN module with this function, but it doesn't work.

Please help.