Part Number: PROCESSOR-SDK-AM62X
Other Parts Discussed in Thread: AM625, SK-AM62
Hi team,
Here's an issue from the customer may need your help:
tar: ./usr/bin/cmake: time stamp 2022-12-14 13:42:04 is 2641.456978585 s in the future tar: ./usr/bin/containerd: time stamp 2022-12-14 14:58:23 is 7218.651506035 s in the future [ 2860.981392] mmc0: running CQE recovery [ 2860.996979] mmc0: running CQE recovery [ 2860.998313] mmc0: running CQE recovery [ 2860.999370] mmc0: running CQE recovery [ 2861.000970] mmc0: running CQE recovery [ 2861.006289] mmc0: running CQE recovery [ 2861.007324] mmc0: running CQE recovery [ 2861.008954] mmc0: running CQE recovery [ 2861.015265] mmc0: running CQE recovery [ 2861.031938] mmc0: running CQE recovery [ 2861.032945] print_req_error: 25 callbacks suppressed [ 2861.032963] blk_update_request: I/O error, dev mmcblk0, sector 17069024 op 0x1:(WRITE) flags 0x4000 phys_seg 17 prio class 0 [ 2861.033244] mmc0: running CQE recovery [ 2861.034284] blk_update_request: I/O error, dev mmcblk0, sector 17070048 op 0x1:(WRITE) flags 0x4000 phys_seg 17 prio class 0 [ 2861.045853] mmc0: running CQE recovery [ 2861.053873] mmc0: running CQE recovery [ 2861.058818] blk_update_request: I/O error, dev mmcblk0, sector 17068000 op 0x1:(WRITE) flags 0x4000 phys_seg 17 prio class 0 [ 2861.068269] mmc0: running CQE recovery [ 2861.076576] mmc0: running CQE recovery [ 2861.081737] mmc0: running CQE recovery [ 2861.082929] mmc0: running CQE recovery [ 2861.099754] EXT4-fs warning: 13 callbacks suppressed [ 2861.099777] EXT4-fs warning (device mmcblk0p1): ext4_end_bio:347: I/O error 10 writing to inode 523442 starting block 2133925) [ 2861.099922] buffer_io_error: 11640 callbacks suppressed [ 2861.099930] Buffer I/O error on device mmcblk0p1, logical block 2132860 [ 2861.099958] Buffer I/O error on device mmcblk0p1, logical block 2132861 [ 2861.099964] Buffer I/O error on device mmcblk0p1, logical block 2132862 [ 2861.099971] Buffer I/O error on device mmcblk0p1, logical block 2132863 [ 2861.099978] Buffer I/O error on device mmcblk0p1, logical block 2132864 [ 2861.099985] Buffer I/O error on device mmcblk0p1, logical block 2132865 [ 2861.099992] Buffer I/O error on device mmcblk0p1, logical block 2132866 [ 2861.099998] Buffer I/O error on device mmcblk0p1, logical block 2132867 tar: [ 2861.100004] Buffer I/O error on device mmcblk0p1, logical block 2132868 ./usr/bin/containerd-ctr: time stamp 2022-12-14 14:58:23 is 7217[ 2861.100011] Buffer I/O error on device mmcblk0p1, logical block 2132869 .69618382 s in the future [ 2861.101556] mmc0: running CQE recovery [ 2861.106140] blk_update_request: I/O error, dev mmcblk0, sector 17056824 op 0x1:(WRITE) flags 0x4000 phys_seg 82 prio class 0 [ 2861.106728] mmc0: running CQE recovery [ 2861.110588] mmc0: running CQE recovery [ 2861.117495] blk_update_request: I/O error, dev mmcblk0, sector 17061192 op 0x1:(WRITE) flags 0x4000 phys_seg 15 prio class 0 [ 2861.118818] mmc0: running CQE recovery [ 2861.125939] mmc0: running CQE recovery [ 2861.127420] mmc0: running CQE recovery [ 2861.128237] blk_update_request: I/O error, dev mmcblk0, sector 17064264 op 0x1:(WRITE) flags 0x0 phys_seg 24 prio class 0 [ 2861.129562] mmc0: running CQE recovery tar: ./usr/bin/containerd-shim: time stamp 2022-12-14 14:58:23 is 7217.36616946 s in the future tar: ./usr/bin/cpack: time stamp 2022-12-14 13:42:04 is 2637.968259065 s in the future tar: ./usr/bin/cpp: time stamp 2022-12-14 13:52:00 is 3233.967577875 s in the future tar: ./usr/bin/crossscripts: time stamp 2022-12-14 13:13:06 is 899.94117555 s in the future tar: ./usr/bin/cryptdir: time stamp 2022-12-14 13:16:31 is 1104.94076695 s in the future tar: ./usr/bin/ctest: time stamp 2022-12-14 13:42:04 is 2637.70119498 s in the future tar: ./usr/bin/cvtsudoers: time stamp 2022-12-14 12:59:08 is 61.66823581 s in the future tar: ./usr/bin/decryptdir: time stamp 2022-12-14 13:16:31 is 1104.63633819 s in the future tar: ./usr/bin/dislocate: time stamp 2022-12-14 13:16:31 is 1104.612384365 s in the future tar: ./usr/bin/docker: time stamp 2022-12-14 15:00:39 is 7350.278375805 s in the future [ 2921.498239] mmc0: cqhci: timeout for tag 25 [ 2921.498266] mmc0: cqhci: ============ CQHCI REGISTER DUMP =========== [ 2921.498270] mmc0: cqhci: Caps: 0x000030c8 | Version: 0x00000510 [ 2921.498276] mmc0: cqhci: Config: 0x00000101 | Control: 0x00000000 [ 2921.498281] mmc0: cqhci: Int stat: 0x00000000 | Int enab: 0x00000006 [ 2921.498285] mmc0: cqhci: Int sig: 0x00000006 | Int Coal: 0x00000000 [ 2921.498289] mmc0: cqhci: TDL base: 0x80ef9000 | TDL up32: 0x00000000 [ 2921.498293] mmc0: cqhci: Doorbell: 0xffffffff | TCN: 0x00000000 [ 2921.498298] mmc0: cqhci: Dev queue: 0x00000000 | Dev Pend: 0x00000000 [ 2921.498302] mmc0: cqhci: Task clr: 0x00000000 | SSC1: 0x00011000 [ 2921.498307] mmc0: cqhci: SSC2: 0x00000001 | DCMD rsp: 0x00000000 [ 2921.498311] mmc0: cqhci: RED mask: 0xfdf9a080 | TERRI: 0x872f052c [ 2921.498316] mmc0: cqhci: Resp idx: 0x0000002d | Resp arg: 0x00000d00 [ 2921.498320] mmc0: sdhci: ============ SDHCI REGISTER DUMP =========== [ 2921.498325] mmc0: sdhci: Sys addr: 0x00000400 | Version: 0x00001004 [ 2921.498329] mmc0: sdhci: Blk size: 0x00007080 | Blk cnt: 0x00000000 [ 2921.498334] mmc0: sdhci: Argument: 0x00000000 | Trn mode: 0x00000013 [ 2921.498338] mmc0: sdhci: Present: 0x01ff00f0 | Host ctl: 0x0000003c [ 2921.498343] mmc0: sdhci: Power: 0x0000000f | Blk gap: 0x00000080 [ 2921.498347] mmc0: sdhci: Wake-up: 0x00000000 | Clock: 0x00000007 [ 2921.498351] mmc0: sdhci: Timeout: 0x0000000e | Int stat: 0x00000000 [ 2921.498355] mmc0: sdhci: Int enab: 0x02ff4000 | Sig enab: 0x02ff4000 [ 2921.498359] mmc0: sdhci: ACmd stat: 0x00000000 | Slot int: 0x00000000 [ 2921.498363] mmc0: sdhci: Caps: 0x3decc801 | Caps_1: 0x18002407 [ 2921.498367] mmc0: sdhci: Cmd: 0x0000153a | Max curr: 0x00000000 [ 2921.498372] mmc0: sdhci: Resp[0]: 0x00000900 | Resp[1]: 0xffc003ff [ 2921.498377] mmc0: sdhci: Resp[2]: 0x328f5903 | Resp[3]: 0x00d07f01 [ 2921.498380] mmc0: sdhci: Host ctl2: 0x0000000b [ 2921.498384] mmc0: sdhci: ADMA Err: 0x00000000 | ADMA Ptr: 0x0000000081e5720c [ 2921.498389] mmc0: sdhci: ============================================ [ 2921.498424] mmc0: running CQE recovery [ 2921.504462] mmc0: running CQE recovery [ 2921.515617] mmc0: running CQE recovery [ 2921.520871] mmc0: running CQE recovery [ 2921.550551] mmc0: running CQE recovery [ 2921.559104] mmc0: running CQE recovery [ 2921.569970] mmc0: running CQE recovery [ 2921.577616] mmc0: running CQE recovery [ 2921.582919] mmc0: running CQE recovery [ 2921.584175] mmc0: running CQE recovery [ 2921.585363] mmc0: running CQE recovery [ 2921.586225] blk_update_request: I/O error, dev mmcblk0, sector 17057848 op 0x1:(WRITE) flags 0x4000 phys_seg 91 prio class 0 [ 2921.586249] EXT4-fs warning (device mmcblk0p1): ext4_end_bio:347: I/O error 10 writing to inode 523440 starting block 2132377) [ 2921.586303] blk_update_request: I/O error, dev mmcblk0, sector 17062216 op 0x1:(WRITE) flags 0x4000 phys_seg 24 prio class 0 [ 2982.938220] mmc0: cqhci: timeout for tag 0 [ 2982.938251] mmc0: cqhci: ============ CQHCI REGISTER DUMP =========== [ 2982.938256] mmc0: cqhci: Caps: 0x000030c8 | Version: 0x00000510 [ 2982.938261] mmc0: cqhci: Config: 0x00000101 | Control: 0x00000000 [ 2982.938266] mmc0: cqhci: Int stat: 0x00000000 | Int enab: 0x00000006 [ 2982.938270] mmc0: cqhci: Int sig: 0x00000006 | Int Coal: 0x00000000 [ 2982.938274] mmc0: cqhci: TDL base: 0x80ef9000 | TDL up32: 0x00000000 [ 2982.938279] mmc0: cqhci: Doorbell: 0xffffffff | TCN: 0x00000000 [ 2982.938283] mmc0: cqhci: Dev queue: 0x00000000 | Dev Pend: 0x00000000 [ 2982.938287] mmc0: cqhci: Task clr: 0x00000000 | SSC1: 0x00011000 [ 2982.938292] mmc0: cqhci: SSC2: 0x00000001 | DCMD rsp: 0x00000000 [ 2982.938296] mmc0: cqhci: RED mask: 0xfdf9a080 | TERRI: 0x992f1a2c [ 2982.938301] mmc0: cqhci: Resp idx: 0x0000002f | Resp arg: 0x00000900 [ 2982.938306] mmc0: sdhci: ============ SDHCI REGISTER DUMP =========== [ 2982.938311] mmc0: sdhci: Sys addr: 0x00000400 | Version: 0x00001004 [ 2982.938315] mmc0: sdhci: Blk size: 0x00007080 | Blk cnt: 0x00000000 [ 2982.938320] mmc0: sdhci: Argument: 0x00000000 | Trn mode: 0x00000013 [ 2982.938324] mmc0: sdhci: Present: 0x01ff00f0 | Host ctl: 0x0000003c [ 2982.938329] mmc0: sdhci: Power: 0x0000000f | Blk gap: 0x00000080 [ 2982.938334] mmc0: sdhci: Wake-up: 0x00000000 | Clock: 0x00000007 [ 2982.938339] mmc0: sdhci: Timeout: 0x0000000e | Int stat: 0x00000000 [ 2982.938343] mmc0: sdhci: Int enab: 0x02ff4000 | Sig enab: 0x02ff4000 [ 2982.938348] mmc0: sdhci: ACmd stat: 0x00000000 | Slot int: 0x00000000 [ 2982.938352] mmc0: sdhci: Caps: 0x3decc801 | Caps_1: 0x18002407 [ 2982.938357] mmc0: sdhci: Cmd: 0x0000153a | Max curr: 0x00000000 [ 2982.938361] mmc0: sdhci: Resp[0]: 0x00000900 | Resp[1]: 0xffc003ff [ 2982.938365] mmc0: sdhci: Resp[2]: 0x328f5903 | Resp[3]: 0x00d07f01 [ 2982.938369] mmc0: sdhci: Host ctl2: 0x0000000b [ 2982.938373] mmc0: sdhci: ADMA Err: 0x00000000 | ADMA Ptr: 0x0000000081e5720c [ 2982.938378] mmc0: sdhci: ============================================ [ 2982.938447] mmc0: running CQE recovery [ 2982.955917] mmc0: running CQE recovery [ 2982.980064] mmc0: running CQE recovery [ 2982.986814] mmc0: running CQE recovery [ 3044.378219] mmc0: cqhci: timeout for tag 0 [ 3044.378248] mmc0: cqhci: ============ CQHCI REGISTER DUMP =========== [ 3044.378251] mmc0: cqhci: Caps: 0x000030c8 | Version: 0x00000510 [ 3044.378256] mmc0: cqhci: Config: 0x00000101 | Control: 0x00000000 [ 3044.378261] mmc0: cqhci: Int stat: 0x00000000 | Int enab: 0x00000006 [ 3044.378265] mmc0: cqhci: Int sig: 0x00000006 | Int Coal: 0x00000000 [ 3044.378269] mmc0: cqhci: TDL base: 0x80ef9000 | TDL up32: 0x00000000 [ 3044.378274] mmc0: cqhci: Doorbell: 0xffffffff | TCN: 0x00000000 [ 3044.378278] mmc0: cqhci: Dev queue: 0x00000000 | Dev Pend: 0x00000000 [ 3044.378282] mmc0: cqhci: Task clr: 0x00000000 | SSC1: 0x00011000 [ 3044.378286] mmc0: cqhci: SSC2: 0x00000001 | DCMD rsp: 0x00000000 [ 3044.378290] mmc0: cqhci: RED mask: 0xfdf9a080 | TERRI: 0x9e2f182c [ 3044.378295] mmc0: cqhci: Resp idx: 0x0000002f | Resp arg: 0x00000900 [ 3044.378300] mmc0: sdhci: ============ SDHCI REGISTER DUMP =========== [ 3044.378305] mmc0: sdhci: Sys addr: 0x00000400 | Version: 0x00001004 [ 3044.378309] mmc0: sdhci: Blk size: 0x00007080 | Blk cnt: 0x00000000 [ 3044.378313] mmc0: sdhci: Argument: 0x00000000 | Trn mode: 0x00000013 [ 3044.378318] mmc0: sdhci: Present: 0x01ff00f0 | Host ctl: 0x0000003c [ 3044.378322] mmc0: sdhci: Power: 0x0000000f | Blk gap: 0x00000080 [ 3044.378326] mmc0: sdhci: Wake-up: 0x00000000 | Clock: 0x00000007 [ 3044.378331] mmc0: sdhci: Timeout: 0x0000000e | Int stat: 0x00000000 [ 3044.378335] mmc0: sdhci: Int enab: 0x02ff4000 | Sig enab: 0x02ff4000 [ 3044.378339] mmc0: sdhci: ACmd stat: 0x00000000 | Slot int: 0x00000000 [ 3044.378343] mmc0: sdhci: Caps: 0x3decc801 | Caps_1: 0x18002407 [ 3044.378347] mmc0: sdhci: Cmd: 0x0000153a | Max curr: 0x00000000 [ 3044.378352] mmc0: sdhci: Resp[0]: 0x00000900 | Resp[1]: 0xffc003ff [ 3044.378356] mmc0: sdhci: Resp[2]: 0x328f5903 | Resp[3]: 0x00d07f01 [ 3044.378360] mmc0: sdhci: Host ctl2: 0x0000000b [ 3044.378365] mmc0: sdhci: ADMA Err: 0x00000000 | ADMA Ptr: 0x0000000081e5720c [ 3044.378369] mmc0: sdhci: ============================================ [ 3044.378434] mmc0: running CQE recovery [ 3044.381981] mmc0: running CQE recovery [ 3044.400848] mmc0: running CQE recovery [ 3044.411171] mmc0: running CQE recovery [ 3044.413504] mmc0: running CQE recovery [ 3044.417729] mmc0: running CQE recovery [ 3044.425287] blk_update_request: I/O error, dev mmcblk0, sector 17089480 op 0x1:(WRITE) flags 0x4000 phys_seg 27 prio class 0 [ 3044.434580] mmc0: running CQE recovery [ 3044.440631] mmc0: running CQE recovery [ 3044.442099] mmc0: running CQE recovery [ 3044.465522] mmc0: running CQE recovery [ 3044.467840] mmc0: running CQE recovery [ 3044.469968] mmc0: running CQE recovery [ 3044.476961] blk_update_request: I/O error, dev mmcblk0, sector 17063240 op 0x1:(WRITE) flags 0x4000 phys_seg 49 prio class 0 [ 3044.476991] EXT4-fs warning (device mmcblk0p1): ext4_end_bio:347: I/O error 10 writing to inode 523441 starting block 2133116) [ 3044.478489] mmc0: running CQE recovery
SDK: 08.05.00.21 release of Processor SDK RT-Linux for AM62x
Using the official AM62x development board.
When extracting the root file system from SD card to EMMC using tar, an error interrupt is reported after 4-5 minutes of extracting, as shown above. This error also occurs when they try to copy the file in the SD card root directory with the CP command. The customer also tried to repartition and format EMMC but all failed.
The kernel image and root file system used are provided by default. This issue has been verified on both Demo boards. The extracted file can be a compressed package of the default root file system: Tisdk-default-image-am62xx-EVM.tar.xz; OR it can be a self-made compressed file.
And the issue will be present whenever extracted to EMMC, but it is not the case on the SD card.
The customer would like to know the possible cause of this issue. Thanks.
Best Regards,
Cherry