Part Number: AM3351
Hi
I am seeing some kernel crash in bootup log. I did not get why this loges are coming.
Can you please help here bellow are the loges.
[ 0.166044] l3-aon-clkctrl:0000:0: failed to disable
[ 0.172358] l4ls-clkctrl:0088:0: failed to enable
[ 0.172417] ------------[ cut here ]------------
[ 0.172487] WARNING: CPU: 0 PID: 1 at drivers/clk/clk.c:958 clk_core_disable+0xc4/0xcc
[ 0.172505] l4ls-clkctrl:0088:0 already disabled
[ 0.172519] Modules linked in:
[ 0.172559] CPU: 0 PID: 1 Comm: swapper Not tainted 5.4.106-g9f48a2ac05 #1
[ 0.172576] Hardware name: Generic AM33XX (Flattened Device Tree)
[ 0.172646] [<c010db78>] (unwind_backtrace) from [<c010b2f0>] (show_stack+0x10/0x14)
[ 0.172700] [<c010b2f0>] (show_stack) from [<c07f3648>] (__warn+0xd0/0xe8)
[ 0.172742] [<c07f3648>] (__warn) from [<c07f36f8>] (warn_slowpath_fmt+0x98/0xc8)
[ 0.172783] [<c07f36f8>] (warn_slowpath_fmt) from [<c041aa74>] (clk_core_disable+0xc4/0xcc)
[ 0.172823] [<c041aa74>] (clk_core_disable) from [<c041ae54>] (clk_core_disable_lock+0x18/0x24)
[ 0.172878] [<c041ae54>] (clk_core_disable_lock) from [<c0118c6c>] (_disable_clocks+0x18/0x98)
[ 0.172916] [<c0118c6c>] (_disable_clocks) from [<c011964c>] (_idle+0x180/0x250)
[ 0.172947] [<c011964c>] (_idle) from [<c011a224>] (_setup.part.0+0x35c/0x504)
[ 0.172994] [<c011a224>] (_setup.part.0) from [<c0c0b26c>] (__omap_hwmod_setup_all+0x114/0x128)
[ 0.173038] [<c0c0b26c>] (__omap_hwmod_setup_all) from [<c0102648>] (do_one_initcall+0x58/0x1c4)
[ 0.173089] [<c0102648>] (do_one_initcall) from [<c0c00ee4>] (kernel_init_freeable+0x124/0x1c0)
[ 0.173142] [<c0c00ee4>] (kernel_init_freeable) from [<c07fc134>] (kernel_init+0x8/0x110)
[ 0.173178] [<c07fc134>] (kernel_init) from [<c01010e8>] (ret_from_fork+0x14/0x2c)
[ 0.173198] Exception stack(0xee883fb0 to 0xee883ff8)
[ 0.173229] 3fa0: 00000000 00000000 00000000 00000000
[ 0.173263] 3fc0: 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
[ 0.173294] 3fe0: 00000000 00000000 00000000 00000000 00000013 00000000
[ 0.173331] ---[ end trace fef1a771dfed0463 ]---
[ 0.178956] l4ls-clkctrl:008c:0: failed to enable
[ 0.179029] ------------[ cut here ]------------
[ 0.179067] WARNING: CPU: 0 PID: 1 at drivers/clk/clk.c:958 clk_core_disable+0xc4/0xcc
[ 0.179084] l4ls-clkctrl:008c:0 already disabled
[ 0.179096] Modules linked in:
[ 0.179127] CPU: 0 PID: 1 Comm: swapper Tainted: G W 5.4.106-g9f48a2ac05 #1
[ 0.179144] Hardware name: Generic AM33XX (Flattened Device Tree)
[ 0.179186] [<c010db78>] (unwind_backtrace) from [<c010b2f0>] (show_stack+0x10/0x14)
[ 0.179225] [<c010b2f0>] (show_stack) from [<c07f3648>] (__warn+0xd0/0xe8)
[ 0.179263] [<c07f3648>] (__warn) from [<c07f36f8>] (warn_slowpath_fmt+0x98/0xc8)
[ 0.179303] [<c07f36f8>] (warn_slowpath_fmt) from [<c041aa74>] (clk_core_disable+0xc4/0xcc)
[ 0.179340] [<c041aa74>] (clk_core_disable) from [<c041ae54>] (clk_core_disable_lock+0x18/0x24)
[ 0.179379] [<c041ae54>] (clk_core_disable_lock) from [<c0118c6c>] (_disable_clocks+0x18/0x98)
[ 0.179414] [<c0118c6c>] (_disable_clocks) from [<c011964c>] (_idle+0x180/0x250)
[ 0.179444] [<c011964c>] (_idle) from [<c011a224>] (_setup.part.0+0x35c/0x504)
[ 0.179480] [<c011a224>] (_setup.part.0) from [<c0c0b26c>] (__omap_hwmod_setup_all+0x114/0x128)
[ 0.179517] [<c0c0b26c>] (__omap_hwmod_setup_all) from [<c0102648>] (do_one_initcall+0x58/0x1c4)
[ 0.179555] [<c0102648>] (do_one_initcall) from [<c0c00ee4>] (kernel_init_freeable+0x124/0x1c0)
[ 0.179594] [<c0c00ee4>] (kernel_init_freeable) from [<c07fc134>] (kernel_init+0x8/0x110)
[ 0.179628] [<c07fc134>] (kernel_init) from [<c01010e8>] (ret_from_fork+0x14/0x2c)
[ 0.179647] Exception stack(0xee883fb0 to 0xee883ff8)
[ 0.179673] 3fa0: 00000000 00000000 00000000 00000000
[ 0.179707] 3fc0: 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
[ 0.179737] 3fe0: 00000000 00000000 00000000 00000000 00000013 00000000
[ 0.179755] ---[ end trace fef1a771dfed0464 ]---
[ 0.182992] cpuidle: using governor ladder
[ 0.183073] cpuidle: using governor menu
Thank You, Jit