Hi,
IBIS model of AM1808 or OmapL138 processor does not have adequate information for DDR2 simulation.
Because : In IBIS file contains BSSTL18TCSCGPBFZ Model selector and it consist of only Fast Mode of NOSR0_NOTERM_1P8 (%10 variation) and
NOSR0_NOTERM_0.1_1P8 (100mV variation). I did not understand why it is FAST, what the mean of FAST? Which model does it correspond to in page 46
of DDR2/mDDR user guide.
This page shows that 2 drive strentgth (Normal and Weak) of DDR2 and
4 drive strength (Full, 1/2, 1/4 and 3/4) of mDDR. These drive strength should be contained in the model selection of IBIS model like other microprocessor IBIS model.
This is not a case for DDR2 ICs. Because of its IBIS model contains FULL and HALF model.
I wonder any users of AM1808 does not need to IBIS model, or TI did not noticed so far (!!!). (For example LogicPD or Spectrum Digital , does not use IBIS model for signal integrity simulation on own board? It is so interesting. Because of datasheet contains generic placement and constraints.
Thanks for your answers.
Best Regards,
FERHAT YALDIZ