Part Number: PROCESSOR-SDK-AM62A
Hi all,
I am trying to display a video captured using a USB camera - LI-IMX424-GW5400-FPDLINKIII
using the HDMI output port.
I have managed to make it work using a standard Logitec webcam withthe following Gstreamer command:
gst-launch-1.0 v4l2src device="/dev/video2" ! video/x-raw, width=1024, height=576, framerate=15/1 ! kmssink driver-name=tidss
It work well, except that the default app is still running in the background (this is not the issue).
root@am62axx-evm:/opt/edgeai-gst-apps# v4l2-ctl --list-formats -d /dev/video2
[ 3991.305180] uvcvideo: Failed to query (GET_DEF) UVC control 7 on unit 2: -32 (exp. 2).
[ 3991.313382] uvcvideo: Failed to query (GET_DEF) UVC control 7 on unit 2: -32 (exp. 2).
[ 3991.322463] uvcvideo: Failed to query (GET_DEF) UVC control 7 on unit 2: -32 (exp. 2).
[ 3991.330890] uvcvideo: Failed to query (GET_DEF) UVC control 7 on unit 2: -32 (exp. 2).
[ 3991.339324] uvcvideo: Failed to query (GET_DEF) UVC control 7 on unit 2: -32 (exp. 2).
[ 3991.347592] uvcvideo: Failed to query (GET_DEF) UVC control 11 on unit 2: -32 (exp. 1).
[ 3991.356095] uvcvideo: Failed to query (GET_DEF) UVC control 9 on unit 2: -32 (exp. 2).
[ 3991.365018] uvcvideo: Failed to query (GET_DEF) UVC control 5 on unit 2: -32 (exp. 1).
[ 3991.373226] uvcvideo: Failed to query (GET_CUR) UVC control 11 on unit 2: -32 (exp. 1).
ioctl: VIDIOC_ENUM_FMT
Type: Video Capture
[0]: 'YUYV' (YUYV 4:2:2)
gst-launch-1.0 v4l2src device="/dev/video2" ! video/x-raw, width=640, height=480 ! kmssink driver-name=tidss