Hello TI experts,
I configured the transmitter of McBSP1 on C6655 as follows:
- 1 phase
- 1 element in phase 1
- The size of the element is 16-bit
- The internal clock is used to generate the clock and frame sync signals.
I used the oscilloscope to measure the DX and FSX pins. Please see the below image. (CH1 is the frame sync, Ch2 is the data:0xA5A5)
Are these signals acceptable? Is there any solution to reduce the overshoot?
Thanks.