Part Number: AM625
Hi,
SDK:ti-processor-sdk-linux-am62xx-evm-08.03.00.19
Custom board
Customer wants to boot from uart, uart prints 01000000011a0000616d36327800000000000000475020200100010001000100CCCCCCCCCCCCCC"
Then use SecureCRT's xmodem to transmit the prebuild image tiboot3:
Starting xmodem transfer. Press Ctrl+C to cancel.
Transferring tiboot3.bin...
100% 327 KB 7 KB/sec 00:00:45 0 Errors
After waiting for a few minutes, the following appears again:
01000000011a0000616d36327800000000000000475020200100010001000100CCCCCCCCCCCCCC
If using the tiboot3 compiled by himself:
Starting xmodem transfer. Press Ctrl+C to cancel.
Transferring tiboot3.bin...
100% 327 KB 7 KB/sec 00:00:45 0 Errors
After that, the uart has no output
Tispl.bin unable to download. Please help check.