This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA2P-ACD: TDA2P-ACD DSS video output performance with horizontal pixel amount over 1920

Part Number: TDA2P-ACD

Dear TI colleague,

since TDA2P-ACD can support the max. graphics processing 1920*1080 with 60fps according to the datasheet

I want to ask if TDA2P-ACD can support the video stream output via parallel link with the following parameter

Resolution: 1969 x 756 (which is little bit over 1920)

Stream Type: YUV 422

Fps: 30

btw. what would be the max. transferred horizontal pixel in this case ?

Look forward to your reply 

many thanks and BR