Dear!
When I run the example of "C:\Program Files\Texas Instruments\quickStartOMAPL1x_rCSL\OMAPL1x\rCSL_examples\evmOMAPL138\ARM_examples\timer\TIMER_interrupt_armL138".
In the function "static void init_OMAPL138 (void)",I step into/over the statement "_call_swi(ARM_PRIV_MODE_KEY);".The PC is always jump to 0x00000008. I found in the command file OMAPL138_ARM.cmd,the linker put the section .intvecs to ARM's RAM 0xFFFF0000.
I'm confused that why the PC don't jump to 0xFFFF0000 when step into "_call_swi(ARM_PRIV_MODE_KEY);".
In OMAPL138_ARM.cmd,I also don't understand the statements "--retain=INT_VECS and --diag_remark=10063"
In this project, I didn't use the ARM side .gel files .Because My OMAPL138 don't have ARM side .gel file.
Thanks for everyone's time and help!



, then the program directly run to main().


and push the Reset button on my board,