This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA4VM: Boot uboot from EMMC fail

Part Number: TDA4VM


Hi, experts ,

 I refer to FAQ] PROCESSOR-SDK-DRA8X-TDA4X: Boot uboot from EMMC - Processors forum - Processors - TI E2E support forums write the images to eMMC(SDK 08_04_00) , but  some errors occurred. Details are as

follows,Please help me analyze the reason,thanks!

U-Boot SPL 2021.01 (Feb 02 2023 - 15:20:52 +0800)
Model: Texas Instruments K3 J721E SoC
SYSFW ABI: 3.1 (firmware rev 0x0008 '8.4.1--v08.04.01 (Jolly Jellyfi')
Trying to boot from MMC1
mmc_load_image_raw_sector: mmc block read error
** Partition 1 not valid on device 0 **
spl_register_fat_device: fat register err - -1
spl_load_image_fat: error reading image tispl.bin, err - -1
spl: no partition table found
SPL: failed to boot from all boot devices
### ERROR ### Please RESET the board ###

Best Regards,

Bing